USB-OTG to setup serial console (minicom)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB-OTG to setup serial console (minicom)

2,014 次查看
srinivasaporam
Contributor II

Hi,

We have got new IMX6 board (customized based on reference design-SABRELite) which has come after assembly. Now we are trying port Uboot, Kernel and OS to this new board.

We came to know that setting up serial console is required to see and change the settings in Uboot. But unfortunately we do not have any serial port (DB9) in the board. Can we use USB (connected to my HOST PC which runs minicom) and OTG (on the board side)  to setup serial console to view boot settins. How this can be done.

标签 (5)
0 项奖励
回复
1 回复

1,413 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Srinavasa

Sabre SD for serial connection with host pc

uses FTDI  FT232RQ (uses PC USB port) iMX6_SABRE_SDB_DESIGNFILES

I am not aware of methods of usage of processor USB OTG for such purposes.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复