LPDDR2 frequency change in imx6solo ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPDDR2 frequency change in imx6solo ?

1,774件の閲覧回数
ela_embedded
Contributor I

we are using micron LPDDR2  interfaced with imx6solo in our customized board . DDR has three modes of speed grade with 533MHZ , 400 MHZ and 333 MHZ  . we need to configure our mmdc to 333MHz  for power optimization . Is this possible ? i have  gone through the reference manual but i didnt found the required information for mmdc.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,689件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ela

yes this is possible, for procedure one can look at attached document

Chapter 21 Dynamic Bus Frequency Driver from L3.14.28_1.0.0_iMX6QDLS_BUNDLE

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信