USB LDO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
2,444 Views
joshk
Contributor I

Hello,

     I have an IMx6SL and would like to know what the USB LDO Register value is so I can modify the voltage in 25mV steps as outlined in the manual 36.4 USB LDO Regulator

Thank you!

~Josh

Labels (1)
0 Kudos
Reply
1 Solution
2,345 Views
igorpadykov
NXP Employee
NXP Employee

Hi Josh

as PMU is similar to i.MX6DQ, one can use description in

sect.50.7.2 Regulator 3P0 Register (PMU_REG_3P0) IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,346 Views
igorpadykov
NXP Employee
NXP Employee

Hi Josh

as PMU is similar to i.MX6DQ, one can use description in

sect.50.7.2 Regulator 3P0 Register (PMU_REG_3P0) IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,345 Views
joshk
Contributor I

Thanks, I was guessing this was the correct register after looking at the SDK but this clarifies everything! :smileyhappy:

0 Kudos
Reply