USB LDO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,448件の閲覧回数
joshk
Contributor I

Hello,

     I have an IMx6SL and would like to know what the USB LDO Register value is so I can modify the voltage in 25mV steps as outlined in the manual 36.4 USB LDO Regulator

Thank you!

~Josh

ラベル(1)
0 件の賞賛
返信
1 解決策
2,349件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Josh

as PMU is similar to i.MX6DQ, one can use description in

sect.50.7.2 Regulator 3P0 Register (PMU_REG_3P0) IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,350件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Josh

as PMU is similar to i.MX6DQ, one can use description in

sect.50.7.2 Regulator 3P0 Register (PMU_REG_3P0) IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,349件の閲覧回数
joshk
Contributor I

Thanks, I was guessing this was the correct register after looking at the SDK but this clarifies everything! :smileyhappy:

0 件の賞賛
返信