USB_H1_PWR control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB_H1_PWR control

Jump to solution
2,718 Views
Kazuma_Sasaki
Senior Contributor I

Moving to new thread:

Hi Igor,

 

From RM:

pastedImage_1.png

 

- We are configuring EIM_D31 pad as USB_H1_PWR function.

- EIM_D31 pad is connecting to enable pad of power IC for cutting VBUS supply.

- When iMX6 detect over-current event, I am expecting EIM_D31 output high signal. 

 

I would like to know the control procedure outputting  a high signal from EIM_D31 pad with USB_H1_PWR function.

 

Best Regards,

Kazuma Sasaki.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,671 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

according to below link nxp bsps use simple gpio for control of that signal

How to control the USB_OTG_PWR and the USB_H1_PWR of i.MX6 

In general PP bit in USB_nPORTSC1 register also can be used, details can be

found in sect.65.4.3.2.4 Port Power i.MX 6Solo/6DualLite Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,672 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

according to below link nxp bsps use simple gpio for control of that signal

How to control the USB_OTG_PWR and the USB_H1_PWR of i.MX6 

In general PP bit in USB_nPORTSC1 register also can be used, details can be

found in sect.65.4.3.2.4 Port Power i.MX 6Solo/6DualLite Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,671 Views
Kazuma_Sasaki
Senior Contributor I

Hi Igor,

I appreciate your quick response.

I got it. I will try based on your advice.

Best Regards,
Kazuma Sasaki.

0 Kudos
Reply