USB_H1_PWR control

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,800件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

Moving to new thread:

Hi Igor,

 

From RM:

pastedImage_1.png

 

- We are configuring EIM_D31 pad as USB_H1_PWR function.

- EIM_D31 pad is connecting to enable pad of power IC for cutting VBUS supply.

- When iMX6 detect over-current event, I am expecting EIM_D31 output high signal. 

 

I would like to know the control procedure outputting  a high signal from EIM_D31 pad with USB_H1_PWR function.

 

Best Regards,

Kazuma Sasaki.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,753件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

according to below link nxp bsps use simple gpio for control of that signal

How to control the USB_OTG_PWR and the USB_H1_PWR of i.MX6 

In general PP bit in USB_nPORTSC1 register also can be used, details can be

found in sect.65.4.3.2.4 Port Power i.MX 6Solo/6DualLite Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,754件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

according to below link nxp bsps use simple gpio for control of that signal

How to control the USB_OTG_PWR and the USB_H1_PWR of i.MX6 

In general PP bit in USB_nPORTSC1 register also can be used, details can be

found in sect.65.4.3.2.4 Port Power i.MX 6Solo/6DualLite Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,753件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

Hi Igor,

I appreciate your quick response.

I got it. I will try based on your advice.

Best Regards,
Kazuma Sasaki.

0 件の賞賛
返信