USB Camera to Ethernet Video Streaming CPU Load / HW Acceleration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB Camera to Ethernet Video Streaming CPU Load / HW Acceleration

1,631 次查看
brett1
Contributor II

VPU performance: CSI-2 MIPI camera vs. USB camera 

I see this question above with regard to bringing in camera data via USB and streaming it out ethernet taking high CPU resource on the i.MX6.  Is there better hardware acceleration for a task such as this in the i.MX8MMiniLite?  About how much CPU loading would one expect for a lower resolution type say 640X480 compressed stream at 15-30fps?

Thank you!

0 项奖励
回复
1 回复

1,507 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Howard,

The i.MX8M Mini is still on preproduction. In case of requiring support, please directly contact with your Sales or FAE.

Best regards!

/Carlos

0 项奖励
回复