USB Camera to Ethernet Video Streaming CPU Load / HW Acceleration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Camera to Ethernet Video Streaming CPU Load / HW Acceleration

1,658件の閲覧回数
brett1
Contributor II

VPU performance: CSI-2 MIPI camera vs. USB camera 

I see this question above with regard to bringing in camera data via USB and streaming it out ethernet taking high CPU resource on the i.MX6.  Is there better hardware acceleration for a task such as this in the i.MX8MMiniLite?  About how much CPU loading would one expect for a lower resolution type say 640X480 compressed stream at 15-30fps?

Thank you!

0 件の賞賛
返信
1 返信

1,534件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Howard,

The i.MX8M Mini is still on preproduction. In case of requiring support, please directly contact with your Sales or FAE.

Best regards!

/Carlos

0 件の賞賛
返信