USB Camera to Ethernet Video Streaming CPU Load / HW Acceleration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Camera to Ethernet Video Streaming CPU Load / HW Acceleration

1,637 Views
brett1
Contributor II

VPU performance: CSI-2 MIPI camera vs. USB camera 

I see this question above with regard to bringing in camera data via USB and streaming it out ethernet taking high CPU resource on the i.MX6.  Is there better hardware acceleration for a task such as this in the i.MX8MMiniLite?  About how much CPU loading would one expect for a lower resolution type say 640X480 compressed stream at 15-30fps?

Thank you!

0 Kudos
Reply
1 Reply

1,513 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Howard,

The i.MX8M Mini is still on preproduction. In case of requiring support, please directly contact with your Sales or FAE.

Best regards!

/Carlos

0 Kudos
Reply