UART TxD/RxD in DCE mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART TxD/RxD in DCE mode

ソリューションへジャンプ
1,870件の閲覧回数
keitanagashima
Senior Contributor I

Hi.

Refer to 64.2.1.1 Serial/IrDA Signals IMX6SDLRM_Rev.1.

There is description of I/O direction each mode (DCE/DTE).

When I set DCE mode, TxD and RxD became opposite I/O direction.

Is it right operation?

Keita

ラベル(3)
0 件の賞賛
返信
1 解決策
1,614件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please refer to the following FAQ on the Community .

https://community.freescale.com/docs/DOC-97509


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,615件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please refer to the following FAQ on the Community .

https://community.freescale.com/docs/DOC-97509


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信