i.MX6DQ CSI performance.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6DQ CSI performance.

ソリューションへジャンプ
2,188件の閲覧回数
keitanagashima
Senior Contributor I

Hi.

I'd like to know the CSI performance.

Is it possible to input dual 1080p@60 video into CSI?

I think it is impossible.

Because, there is below limitation.

F = FH * FW * FPS * BI * DF

Where

   FH = frame height (in pixels)

   FW = Frame width (in pixels)

   fps = frame rate (frames per second) ? BI = typically 35% overhead, should be assumed as 1.35. The actual blanking intervals are a parameter of the attached device.

   DF = data format, defines the number of cycles needed to send a single pixel.

If one use a 1080p@60 camera;

167.96MHz = 1080 * 1920 * 60 * 1.35 * 1 < 240MHz --> OK

In case of Dual camera;

335.92MHz = 1080 * 1920 * 60 * 1.35 * 1 * 2 > 240MHz --> NG


If one use a 1080p@60 and a 720p@60 camera;

242.6MHz = (1080 * 1920 * 60 * 1.35 * 1) + (1280 * 720 *60 *1.35 * 1) > 240MHz --> NG


Is my understanding right?


Keita


ラベル(3)
0 件の賞賛
返信
1 解決策
1,968件の閲覧回数
Yuri
NXP Employee
NXP Employee

Correct for single IPU.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,969件の閲覧回数
Yuri
NXP Employee
NXP Employee

Correct for single IPU.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,968件の閲覧回数
keitanagashima
Senior Contributor I

Dear Yuri,

Hello.

Thank you for your reply.


>Correct for single IPU.

If one use i.MX6DQ (= 2 IPUs), is it possible to input dual 1080p@60 video?

IPU0 <-- YUV422 1080p@60

IPU1 <-- YUV422 1080p@60

Keita

0 件の賞賛
返信
1,968件の閲覧回数
Yuri
NXP Employee
NXP Employee

Yes.

0 件の賞賛
返信