UART TxD/RxD in DCE mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART TxD/RxD in DCE mode

Jump to solution
1,860 Views
keitanagashima
Senior Contributor I

Hi.

Refer to 64.2.1.1 Serial/IrDA Signals IMX6SDLRM_Rev.1.

There is description of I/O direction each mode (DCE/DTE).

When I set DCE mode, TxD and RxD became opposite I/O direction.

Is it right operation?

Keita

Labels (3)
0 Kudos
Reply
1 Solution
1,604 Views
Yuri
NXP Employee
NXP Employee

Please refer to the following FAQ on the Community .

https://community.freescale.com/docs/DOC-97509


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,605 Views
Yuri
NXP Employee
NXP Employee

Please refer to the following FAQ on the Community .

https://community.freescale.com/docs/DOC-97509


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply