UART RTS/CTS handshaking

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

UART RTS/CTS handshaking

跳至解决方案
3,518 次查看
JamesJukkola
Contributor I

The iMX53 reference manual mentions several times that RTS is an input, and CTS is an output.  However, Table 76-1 on page 4627 shows RTS and CTS changing to input or output based on the DCEDTE bit.  Could someone explain?

标签 (1)
0 项奖励
回复
1 解答
2,435 次查看
Yuri
NXP Employee
NXP Employee

  Please use table 86 in section 4.7.17.1 (UART RS-232 I/O Configuration in Different Modes)
of the Datasheet (IMX53IEC, Rev. 5, 12/2012).
The datasheet relates to the UART + additional signal multiplexing between the UART
peripheral and the IC pad, while the Reference Manual describes only the peripheral boundary

(internal signals).

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,436 次查看
Yuri
NXP Employee
NXP Employee

  Please use table 86 in section 4.7.17.1 (UART RS-232 I/O Configuration in Different Modes)
of the Datasheet (IMX53IEC, Rev. 5, 12/2012).
The datasheet relates to the UART + additional signal multiplexing between the UART
peripheral and the IC pad, while the Reference Manual describes only the peripheral boundary

(internal signals).

0 项奖励
回复