UART RTS/CTS handshaking

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART RTS/CTS handshaking

ソリューションへジャンプ
3,574件の閲覧回数
JamesJukkola
Contributor I

The iMX53 reference manual mentions several times that RTS is an input, and CTS is an output.  However, Table 76-1 on page 4627 shows RTS and CTS changing to input or output based on the DCEDTE bit.  Could someone explain?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,491件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please use table 86 in section 4.7.17.1 (UART RS-232 I/O Configuration in Different Modes)
of the Datasheet (IMX53IEC, Rev. 5, 12/2012).
The datasheet relates to the UART + additional signal multiplexing between the UART
peripheral and the IC pad, while the Reference Manual describes only the peripheral boundary

(internal signals).

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,491件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please use table 86 in section 4.7.17.1 (UART RS-232 I/O Configuration in Different Modes)
of the Datasheet (IMX53IEC, Rev. 5, 12/2012).
The datasheet relates to the UART + additional signal multiplexing between the UART
peripheral and the IC pad, while the Reference Manual describes only the peripheral boundary

(internal signals).

0 件の賞賛
返信