12-bit Bayer RGB format CMos sensor support on i.MX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

12-bit Bayer RGB format CMos sensor support on i.MX6Q

Jump to solution
4,743 Views
FeiShen
NXP Employee
NXP Employee

   Does anyone know how to run 12-bit Bayer RGB format CMos Sensor on i.MX6Q?

   Is the HW connecting method to connect 12-bit data to i.MX6Q, by CSI_DAT[8] to CSI_DAT[19], right?  And, how to convert Bayer RGB format data to RGB / YUV format by i.MX6Q IPU module?

fei.shen@nxp.com
Labels (3)
0 Kudos
Reply
1 Solution
1,696 Views
Yuri
NXP Employee
NXP Employee

For possible sensor connections, please look at the datasheet(s),

for example - Table 64 (Camera Input Signal Cross Reference, Format, and Bits Per Cycle)

of IMX6DQCEC, Rev. 1, 11/2012.

Software operations are described in Platform SDK (IPU driver, IC tasks).


https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null


Also the next may be useful :


https://community.freescale.com/message/309833#309833

View solution in original post

0 Kudos
Reply
1 Reply
1,697 Views
Yuri
NXP Employee
NXP Employee

For possible sensor connections, please look at the datasheet(s),

for example - Table 64 (Camera Input Signal Cross Reference, Format, and Bits Per Cycle)

of IMX6DQCEC, Rev. 1, 11/2012.

Software operations are described in Platform SDK (IPU driver, IC tasks).


https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null


Also the next may be useful :


https://community.freescale.com/message/309833#309833

0 Kudos
Reply