[To Rita Wang] imx8mplus SD boot failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[To Rita Wang] imx8mplus SD boot failure

Jump to solution
2,103 Views
chen-wust
Contributor II

Minimum system change point: Only the power domain of the clk and sdio pins of the SD card boot has been changed from 3.3v to 1.8v. SD card startup without any print information. Hope to get some advice and Pointers.

0 Kudos
Reply
1 Solution
2,073 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You need to use the 1.8V both in the CPU and SD card side, have you use the same design with our reference board? Have you download image to your SD card success and with proper boot mode from SD cards?

View solution in original post

0 Kudos
Reply
2 Replies
2,074 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You need to use the 1.8V both in the CPU and SD card side, have you use the same design with our reference board? Have you download image to your SD card success and with proper boot mode from SD cards?

0 Kudos
Reply
2,054 Views
chen-wust
Contributor II

In previous versions, booting with an sd card was normal, but previous versions used a voltage of 3.3V. Now the clk voltage of the circuit is 1.8v, which cannot be started normally. I am now using uuu boot mode and the kernel will not initialize the sd card properly after burning it. Now I feel that the sd card cannot support 3.3v voltage startup, thank you for your answer

0 Kudos
Reply