I have an Apalis Toradex IMX8 QM Module with an ixora 1.2 carrier board (with a Toradex LVDS Display 10.1) and Im using the tdx-reference-multimedia-image right now. I want to run a QT application on dual Screen(LVDS and HDMI) with Extend Mode!! I try to build and use Qt dual-screen and I would like use “QtWayland” module In the based this link i did All instrutctions but finally when run a qt application(qt-dual-screen-compositor) with 2 pages we faced bellow messages and pages display on active screen(here is HDMI)-2 pages with white color(HDMI-A-1) and red color (LVDS-1) screen page on top of each other:
qt.qpa.wayland: Setting cursor position is not possible on wayland qt.qpa.wayland: Wayland does not support QWindow::requestActivate() qt.qpa.wayland: Wayland does not support QWindow::requestActivate() unable to lock lockfile /run/user/0/wayland-0.lock, maybe another compositor is running
Bytheway I dont have TochScreen(so i didnt do related configuration for lvds and hdmi tochscreen event) and i can’t set position for windows(pages)!! Can you explain Whats solution?? Thank you in advance,