HI igor,
we meet the same issue, also need your support, it is urgent project, tks in advance~
We use the nand flash MT29F32G08CBACAWP. It is found that the CPU cannot output the flash signal. Because the flash port of the CPU can be used as a GPIO function, we used the GPIO function for testing, and the result can output normal high and low levels. But when switching to the flash function, there is still no flash signal output. According to your experience, is it caused by nand flash devices? Or is it caused by PCB line route? Is it necessary to reduce the frequency of nand flash or improve the drive capability of the main control on the flash function? If the nand flash can be read and written correctly in this way, can it be explained that it is caused by the route wiring of the PCB? thank you very much!