Temperature Sensor Calibration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Temperature Sensor Calibration

1,924件の閲覧回数
eishishibusawa
Contributor III

Dear Sir

 

I want to ask you about the Temperature Monitor.

I understand that the Temperature Sensor Calibration Data is stored in OCOTP_ANA1.

It is described at P5172 in IMX6SDLRM Rev.2 as following.

"The temperature calibration values are fused individually for each part in the product testing process."

 

Q1.

Can I understand that the calibration value is written at the factory of NXP?

 

Best Regards,

Eishi SHIBUSAWA

ラベル(2)
0 件の賞賛
返信
1 返信

1,553件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Eishi,

  It means: There is a temperature  sensor in i.MX6 processor, and it's value has been calibrated duiring product testing process.

  In software, for example, in u-boot, linux kernel, it's driver is named "thermal_imx.c", customer can configure MIN temperature and MAX temperature for her application.


Have a great day,
TIC   weidong sun

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信