How to mount the SD card in recovery for Android 6.0.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to mount the SD card in recovery for Android 6.0.1

1,721 次查看
hungjerry
Contributor II

Hi Sir,

   I am use imx6dq with android 6.0.1 and I do like update the image from SD card in recovery mode,

is there any information / guide for that?

                  B.R jerry

标签 (2)
0 项奖励
回复
2 回复数

1,614 次查看
b36401
NXP Employee
NXP Employee

You need to set "recovery" insted of "boot" for booti option in u-boot configuration to enter recovery mode.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,614 次查看
hungjerry
Contributor II

Hi Victor,

   Thanks for suggestion, I have booted to recovery mode and added the option "apply update from SD card" to recovery menu,

but system inform me that there no /scard detected even I put the image files on SD card which format fat or ext4, so I wonder if any guide

to mount SD card in recovery mode.

0 项奖励
回复