Temperature Monitor Block diagram

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Temperature Monitor Block diagram

Jump to solution
2,152 Views
gopinathsriniva
Contributor III

I am checking IMX7D internal temperature sensor section. (Section 14.2) in TRM version "i.MX 7Dual Applications Processor Reference Manual, Rev. 0.1, 08/2016". I found "Figure 14-3. High Level Temp Sensor System Diagram" is missing there. I downloaded the TRM from the below link.

i.MX 7Dual Arm Cortex-A7 Processor|NXP 

I need to check for "High Level Temp Sensor System Diagram". Any help? 

Regards,

Gopinath S

Labels (2)
0 Kudos
Reply
1 Solution
1,993 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

The image will be added in the next RM release.

pastedImage_2.png

For the moment you can use this image as reference.

Best Regards,

Diego

View solution in original post

0 Kudos
Reply
2 Replies
1,994 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

The image will be added in the next RM release.

pastedImage_2.png

For the moment you can use this image as reference.

Best Regards,

Diego

0 Kudos
Reply
1,993 Views
gopinathsriniva
Contributor III

Any updates please? 

0 Kudos
Reply