iMX6UL & PF3000: how to generate the DDR3L VTT for adress termination

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6UL & PF3000: how to generate the DDR3L VTT for adress termination

544 Views
jochenstehle
Contributor III

we use an imx6ul with one DDR3L chip and the PF3000 PMIC. We want to terminate the adressbus but how to generate the 0.675V VTT voltage? Has anyone done a termination in a similar setup?

Labels (3)
0 Kudos
1 Reply

352 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jochen

one can use discrete power components or look at solution

used on i.MX6Q sch-27016 demo sch. For obtaining schematic one

can create service request.  Support|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos