Temperature Monitor Block diagram

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Temperature Monitor Block diagram

ソリューションへジャンプ
2,169件の閲覧回数
gopinathsriniva
Contributor III

I am checking IMX7D internal temperature sensor section. (Section 14.2) in TRM version "i.MX 7Dual Applications Processor Reference Manual, Rev. 0.1, 08/2016". I found "Figure 14-3. High Level Temp Sensor System Diagram" is missing there. I downloaded the TRM from the below link.

i.MX 7Dual Arm Cortex-A7 Processor|NXP 

I need to check for "High Level Temp Sensor System Diagram". Any help? 

Regards,

Gopinath S

ラベル(2)
0 件の賞賛
返信
1 解決策
2,010件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

The image will be added in the next RM release.

pastedImage_2.png

For the moment you can use this image as reference.

Best Regards,

Diego

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,011件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

The image will be added in the next RM release.

pastedImage_2.png

For the moment you can use this image as reference.

Best Regards,

Diego

0 件の賞賛
返信
2,010件の閲覧回数
gopinathsriniva
Contributor III

Any updates please? 

0 件の賞賛
返信