Tamper function in i.MX6.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tamper function in i.MX6.

Jump to solution
3,905 Views
keitanagashima
Senior Contributor I

Hi.

I'd like the sample code of Tamper function for i.MX6.

Does the sample code exist?

Keita

Labels (5)
0 Kudos
Reply
1 Solution
2,373 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

I think they can't be supported.

The Tamper Detection signal is pulled-down internally. In case of use, it should be connected to a Tamper Detection contact in a target system (Normally closed, pulled-up to the VDD_SNVS_IN).

But due to the iMX6 hasn't connected this signal to external IOMUX pad, there is no external pin can be used to connect it to VDD_SNVS_IN.

View solution in original post

0 Kudos
Reply
3 Replies
2,373 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

Although the IMX6 chip supports the tamper function, but we haven't connected the tamper detection pin to IOMUX pad, so the function can't be used.

0 Kudos
Reply
2,373 Views
keitanagashima
Senior Contributor I

Dear Qiang Li,

Thank you for your reply.

I'd like to use tamper detection for Voltage, Temperature, SRTC, Wire mesh.

Are these features supported by i.MX6?

If it is supported, give me sample code.

Keita

0 Kudos
Reply
2,374 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

I think they can't be supported.

The Tamper Detection signal is pulled-down internally. In case of use, it should be connected to a Tamper Detection contact in a target system (Normally closed, pulled-up to the VDD_SNVS_IN).

But due to the iMX6 hasn't connected this signal to external IOMUX pad, there is no external pin can be used to connect it to VDD_SNVS_IN.

0 Kudos
Reply