Tamper function in i.MX6.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tamper function in i.MX6.

ソリューションへジャンプ
5,069件の閲覧回数
keitanagashima
Senior Contributor I

Hi.

I'd like the sample code of Tamper function for i.MX6.

Does the sample code exist?

Keita

ラベル(5)
0 件の賞賛
返信
1 解決策
3,537件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

I think they can't be supported.

The Tamper Detection signal is pulled-down internally. In case of use, it should be connected to a Tamper Detection contact in a target system (Normally closed, pulled-up to the VDD_SNVS_IN).

But due to the iMX6 hasn't connected this signal to external IOMUX pad, there is no external pin can be used to connect it to VDD_SNVS_IN.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,537件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

Although the IMX6 chip supports the tamper function, but we haven't connected the tamper detection pin to IOMUX pad, so the function can't be used.

0 件の賞賛
返信
3,537件の閲覧回数
keitanagashima
Senior Contributor I

Dear Qiang Li,

Thank you for your reply.

I'd like to use tamper detection for Voltage, Temperature, SRTC, Wire mesh.

Are these features supported by i.MX6?

If it is supported, give me sample code.

Keita

0 件の賞賛
返信
3,538件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

I think they can't be supported.

The Tamper Detection signal is pulled-down internally. In case of use, it should be connected to a Tamper Detection contact in a target system (Normally closed, pulled-up to the VDD_SNVS_IN).

But due to the iMX6 hasn't connected this signal to external IOMUX pad, there is no external pin can be used to connect it to VDD_SNVS_IN.

0 件の賞賛
返信