Tamper function in i.MX6.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Tamper function in i.MX6.

跳至解决方案
5,057 次查看
keitanagashima
Senior Contributor I

Hi.

I'd like the sample code of Tamper function for i.MX6.

Does the sample code exist?

Keita

标签 (5)
0 项奖励
回复
1 解答
3,525 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

I think they can't be supported.

The Tamper Detection signal is pulled-down internally. In case of use, it should be connected to a Tamper Detection contact in a target system (Normally closed, pulled-up to the VDD_SNVS_IN).

But due to the iMX6 hasn't connected this signal to external IOMUX pad, there is no external pin can be used to connect it to VDD_SNVS_IN.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,525 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

Although the IMX6 chip supports the tamper function, but we haven't connected the tamper detection pin to IOMUX pad, so the function can't be used.

0 项奖励
回复
3,525 次查看
keitanagashima
Senior Contributor I

Dear Qiang Li,

Thank you for your reply.

I'd like to use tamper detection for Voltage, Temperature, SRTC, Wire mesh.

Are these features supported by i.MX6?

If it is supported, give me sample code.

Keita

0 项奖励
回复
3,526 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

I think they can't be supported.

The Tamper Detection signal is pulled-down internally. In case of use, it should be connected to a Tamper Detection contact in a target system (Normally closed, pulled-up to the VDD_SNVS_IN).

But due to the iMX6 hasn't connected this signal to external IOMUX pad, there is no external pin can be used to connect it to VDD_SNVS_IN.

0 项奖励
回复