System Controller Firmware - Build Environment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

System Controller Firmware - Build Environment

ソリューションへジャンプ
2,197件の閲覧回数
Danilo3
Contributor III

Hello everybody,

I need to customize the SCFW on i.MX8 QuadMax MEK for AAOS 13.0.0_1.1.0, so I downloaded the SCFW porting kit, release Linux LF5.15.71_2.2.0 (as indicated in the "Android Auto User's Guide 13-0-0").

Such porting kit comes with a sc_fw_port.pdf file which claims that the toolchain for compiling the SCFW is the GNU Arm Embedded Toolchain: 8-2018-q4-major December 20, 2018.

On the other hand, I see from the above-mentioned User's Guide that the version of "6-2017-q2-update June 28, 2017" is recommended, as it is verified.

Which one should I choose to avoid any issue?

Thank you

ラベル(1)
0 件の賞賛
返信
1 解決策
2,163件の閲覧回数
Danilo3
Contributor III

Hello @Chavira 

based on your feedback, I will go for version "6-2017-q2-update" as document "Android User's Guide Rev. 13.0.0_1.1.0" is the latest one.

Thank you.

Regards.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,169件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @Danilo3

Thank you for contacting NXP Support!

I recommend following the latest document, all of our documentation is tested before the release.

If you have any problem using the tools you can out your issues in the community or a private case.

 https://www.nxp.com/support/support:SUPPORTHOME

0 件の賞賛
返信
2,164件の閲覧回数
Danilo3
Contributor III

Hello @Chavira 

based on your feedback, I will go for version "6-2017-q2-update" as document "Android User's Guide Rev. 13.0.0_1.1.0" is the latest one.

Thank you.

Regards.

0 件の賞賛
返信