System Controller Firmware - Build Environment

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

System Controller Firmware - Build Environment

跳至解决方案
2,273 次查看
Danilo3
Contributor III

Hello everybody,

I need to customize the SCFW on i.MX8 QuadMax MEK for AAOS 13.0.0_1.1.0, so I downloaded the SCFW porting kit, release Linux LF5.15.71_2.2.0 (as indicated in the "Android Auto User's Guide 13-0-0").

Such porting kit comes with a sc_fw_port.pdf file which claims that the toolchain for compiling the SCFW is the GNU Arm Embedded Toolchain: 8-2018-q4-major December 20, 2018.

On the other hand, I see from the above-mentioned User's Guide that the version of "6-2017-q2-update June 28, 2017" is recommended, as it is verified.

Which one should I choose to avoid any issue?

Thank you

0 项奖励
回复
1 解答
2,239 次查看
Danilo3
Contributor III

Hello @Chavira 

based on your feedback, I will go for version "6-2017-q2-update" as document "Android User's Guide Rev. 13.0.0_1.1.0" is the latest one.

Thank you.

Regards.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,245 次查看
Chavira
NXP TechSupport
NXP TechSupport

Hi @Danilo3

Thank you for contacting NXP Support!

I recommend following the latest document, all of our documentation is tested before the release.

If you have any problem using the tools you can out your issues in the community or a private case.

 https://www.nxp.com/support/support:SUPPORTHOME

0 项奖励
回复
2,240 次查看
Danilo3
Contributor III

Hello @Chavira 

based on your feedback, I will go for version "6-2017-q2-update" as document "Android User's Guide Rev. 13.0.0_1.1.0" is the latest one.

Thank you.

Regards.

0 项奖励
回复