Support for H.264 encoder and decoder in i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Support for H.264 encoder and decoder in i.MX6

1,699 次查看
imx_learner
Contributor I

Hello,

I have a confusion regarding the i.MX6 processors-if they can be used for encoding video data for streaming. The following is an excerpt from the i.MX_VPU_Reference_Manual: 

VPU codec is fully compliant with H.264
BP/MP/HP, VC-1 SP/MP/AP, MPEG-4 SP/ASP except GMC,
DivX (Xvid), MPEG-1/2, VP8, AVS and MJPEG decoding
and H.264, MPEG-4, H.263, and MJPG encoding

I do not understand this statement. VPU codec is compliant with H.264 but not H.264 encoding. What does this mean? 

All the while, I had an idea that the VPU can be used to perform video data compression. 

P.S: My usecase, is to build an embedded video streaming server that sends compressed data wirelessly over WiFi or LTE.

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,390 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi imx learner,

The i.Mx6x has VPU  enconder and decoder, h264 AVC/MVC.

0 项奖励
回复