Support for H.264 encoder and decoder in i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Support for H.264 encoder and decoder in i.MX6

1,707件の閲覧回数
imx_learner
Contributor I

Hello,

I have a confusion regarding the i.MX6 processors-if they can be used for encoding video data for streaming. The following is an excerpt from the i.MX_VPU_Reference_Manual: 

VPU codec is fully compliant with H.264
BP/MP/HP, VC-1 SP/MP/AP, MPEG-4 SP/ASP except GMC,
DivX (Xvid), MPEG-1/2, VP8, AVS and MJPEG decoding
and H.264, MPEG-4, H.263, and MJPG encoding

I do not understand this statement. VPU codec is compliant with H.264 but not H.264 encoding. What does this mean? 

All the while, I had an idea that the VPU can be used to perform video data compression. 

P.S: My usecase, is to build an embedded video streaming server that sends compressed data wirelessly over WiFi or LTE.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,398件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi imx learner,

The i.Mx6x has VPU  enconder and decoder, h264 AVC/MVC.

0 件の賞賛
返信