Strange IfxElementProperty contents when creating plug-in element

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Strange IfxElementProperty contents when creating plug-in element

740件の閲覧回数
YongJunChang
Contributor II

Hi all,

I'm trying to create a buffered-mode plug-in element. I got successfully load the theme in Express as well as the target device with correct preview. As the same as IfxPhotopicker example, the element's size is 144x144. I set the plugin element's property in Express as

In all layouts > Extent Hint > X = 144,

In all layouts > Extent Hint > Y = 144,

In all layouts > Resource > Event Handler = "rearview://"

Everythig looked fine before I checked the pProperty in createElement_rearview(). It says

pProperty has a structure that says mode=0, requiredBufferHeight=0, requiredBufferWidth=144, translucency=144. For some reasons after all, when changeElementMode is called, the pContext has width=1, height=144.

Can anyone have a clue of this problem?

Thanks in advance,

Yong

タグ(2)
0 件の賞賛
返信
0 返答(返信)