Static IP setting and sftp server setting on L5.4.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Static IP setting and sftp server setting on L5.4.3

1,700 Views
molin_du
Contributor II

Hello

I downloaded and burn L5.4 imx-full-image to my imx8qxpmek

--LF_v5.4.y-1.0.0_images_MX8QXPMEK

---- imx-image-full-imx8qxpmek.sdcard

Embedded Linux for i.MX Applications Processors | NXP 

and I had 2 questions in using ftp function.

1. How can I fix a static IP ? which file to modify ?

2. SFTP connection from host PC (FileZilla or gFTP) fail due to below error

   sh: /usr/libexec/sftp-server: No such file or directory

   seems I need to configure sftp server at imx8qxpmek board side, I found some article of reason/solution on CentOS / Ubunt, etc,    however it is not working for imx8qxpmek,  please who know tell me how to do it.

Tags (2)
0 Kudos
Reply
1 Reply

1,648 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the following:

 To set up static IP in MX8M? 

https://community.nxp.com/message/1221183 

Regards,

Yuri.

0 Kudos
Reply