To set up static IP in MX8M?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

To set up static IP in MX8M?

3,943 Views
wjdwogud137
Contributor I

Hi

I want to use MX8M as a static IP.

Use the connmanctl services in the description, but i don't have it.

/etc/network/interaces no files

I wonder how you can give me a static ip.

Thank you

Tags (2)
0 Kudos
Reply
3 Replies

3,853 Views
joanxie
NXP TechSupport
NXP TechSupport

you can try the command like "ifconfig eth0 xx.xx.xx.xx" when board boot up

0 Kudos
Reply

3,853 Views
molin_du
Contributor II

Hello Joan:

Is there any way that the board boot up with a fix IP ? not know how to config poky Linux (on Ubuntu it is easy ... )

0 Kudos
Reply

3,851 Views
joanxie
NXP TechSupport
NXP TechSupport

you can set "ip=static_ip_address" according to the Table 11. Common kernel boot parameters of enclosed file

0 Kudos
Reply