Can use DDR4-2400/2666 for i.mx8m Nano instead of DDR4-3200?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can use DDR4-2400/2666 for i.mx8m Nano instead of DDR4-3200?

858 Views
sharad_yadav
Contributor III

Hello , 

I have question on DDR4 selection. 

Processor datasheet showing DDR4-2400 is supported, but on NXP Eval kit DDR4-3200 (Micron make) is used. 

Can I use part with 2400/2666 MT/S for custom board? What will be impact on processing speed as compare to Eval kit ?

Note - I am using i.MX8M Nano Solo part. 

Regards, 

Sharad

Labels (1)
2 Replies

790 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Sharad,

JEDEC compliant DDR memories allow to work at lower speeds so even though the DDR4-3200 is not supported by the i.MX8M Nano, it can work as a DDR4-2400 so you should have pretty much the same performance when using an actual DDR4-2400 DDR.

I hope this helps!

Regards,

790 Views
sharad_yadav
Contributor III

Thanks gusarambula‌ 

It clears, I can use DDR4 part with 2400/2666 MT/s. 

Regards, 

Sharad

0 Kudos