Solo X Pin to Pin Compatibility

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Solo X Pin to Pin Compatibility

1,503 次查看
infantjesurajf1
Contributor I

The iMX6 series summary sheet (https://www.nxp.com/docs/en/fact-sheet/IMX6SRSFS.pdf) says the SoloX is pin compatible with Dual and Quad versions.
But the summary sheet in this link, https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf says the SoloX is only available in 14 x 14 BGA 0.65 mm pitch, 17 x 17 BGA 0.8 mm pitch, 19 x 19 BGA 0.8 mm pitch” and the higher dual/quad versions are only available in 21 x 21 BGA 0.8 mm pitch.

Can you please confirm if the SoloX is pin to pin compatible with the Dual and Quad versions?

Regards, Infant Jesuraj

标签 (4)
0 项奖励
回复
1 回复

1,411 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The i.MX6SoloX is not pin to pin compatible with the i.MX6Dual and i.MX6Quad in hardware. About the i.MX6SoloX solftware and hardware you can refer to the reference design:

i.MX 6SoloX SABRE Development Board|NXP
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复