Solo X Pin to Pin Compatibility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Solo X Pin to Pin Compatibility

1,504件の閲覧回数
infantjesurajf1
Contributor I

The iMX6 series summary sheet (https://www.nxp.com/docs/en/fact-sheet/IMX6SRSFS.pdf) says the SoloX is pin compatible with Dual and Quad versions.
But the summary sheet in this link, https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf says the SoloX is only available in 14 x 14 BGA 0.65 mm pitch, 17 x 17 BGA 0.8 mm pitch, 19 x 19 BGA 0.8 mm pitch” and the higher dual/quad versions are only available in 21 x 21 BGA 0.8 mm pitch.

Can you please confirm if the SoloX is pin to pin compatible with the Dual and Quad versions?

Regards, Infant Jesuraj

ラベル(4)
0 件の賞賛
返信
1 返信

1,412件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

The i.MX6SoloX is not pin to pin compatible with the i.MX6Dual and i.MX6Quad in hardware. About the i.MX6SoloX solftware and hardware you can refer to the reference design:

i.MX 6SoloX SABRE Development Board|NXP
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信