Setting gstreamer default audio as imx-hdmi-soc instead of wm8962-audio to

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Setting gstreamer default audio as imx-hdmi-soc instead of wm8962-audio to

1,035 次查看
greatcatchen
Contributor I

EVK:imx6q-sabresd
OS:Linux 3.1.53
image:fsl-image-qt5-x11-imx6qdlsolo.sdcard

etc/gconf/gconf.xml.defaults/schemas/system/gstreamer/0.10/default/%gconf.xml
etc/gconf/schemas/gstreamer-0.10.schemas

change form
<default>autoaudiosink</default>
to
<default>autoaudiosink device=hw:1</default>

Is there any better way ?

标签 (2)
0 项奖励
回复
1 回复

874 次查看
Yuri
NXP Employee
NXP Employee

Hello,

The following may help.

https://community.nxp.com/docs/DOC-93745 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复