Setting gstreamer default audio as imx-hdmi-soc instead of wm8962-audio to

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting gstreamer default audio as imx-hdmi-soc instead of wm8962-audio to

1,033 Views
greatcatchen
Contributor I

EVK:imx6q-sabresd
OS:Linux 3.1.53
image:fsl-image-qt5-x11-imx6qdlsolo.sdcard

etc/gconf/gconf.xml.defaults/schemas/system/gstreamer/0.10/default/%gconf.xml
etc/gconf/schemas/gstreamer-0.10.schemas

change form
<default>autoaudiosink</default>
to
<default>autoaudiosink device=hw:1</default>

Is there any better way ?

Labels (2)
0 Kudos
Reply
1 Reply

872 Views
Yuri
NXP Employee
NXP Employee

Hello,

The following may help.

https://community.nxp.com/docs/DOC-93745 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply