Serial Download Example/Instructions or Tool?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Serial Download Example/Instructions or Tool?

23,063件の閲覧回数
Michael_ng
Contributor I

Need to be able to use the serial download (micro usb for example) to boot new executables rather than loading them onto the micro SD...any guidance help would be appreciated.

ラベル(1)
23 返答(返信)

1,114件の閲覧回数
Michael_ng
Contributor I

Yes to your first question... We are building/porting a microkernel to the iMX53 and so are doing bare metal work.  On an M3 which we developed our microkernel on first, we load into flash from eclipse and run from there which is much quicker than installing a new image on the micro sd and booting it that way.  If we can go directly to memory that should work..network boot would likely work too if the bootloader takes care of setting up the drivers for ethernet the way it apparently does for usb and uart?

Thanks for your reply....

0 件の賞賛
返信

1,115件の閲覧回数
RandyKrakora
NXP Employee
NXP Employee

Are you saying you want to load code into RAM via the mfg. tool every time you make a change? Maybe you really want to boot via nfs mounted rfs? Or are you debugging kernel changes? Maybe you can give more details?

0 件の賞賛
返信