ERR006687 Where does GPIO6 go?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ERR006687 Where does GPIO6 go?

跳至解决方案
2,337 次查看
joshuaclayton
Contributor III

Running: custom board with a NovSOM imx6q

I've read ERR006687, and we feel we should do the hardware mod to work around the erratum in the next board revision.

The description says to mux GPIO6 as ethernet interrupt. My question is what should GPIO6 be connected to? Does  it need to be connected to the ethernet phy? Is it already internally connected to the ethernet block in the SoC once muxed?

The EE's are confused.

Thanks,

Joshua

0 项奖励
回复
1 解答
2,077 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Joshua

it can be routed internally using debug signals, as attached

picture shows. For example one can look at

linux-2.6-imx.git - Freescale i.MX Linux Tree

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
2,078 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Joshua

it can be routed internally using debug signals, as attached

picture shows. For example one can look at

linux-2.6-imx.git - Freescale i.MX Linux Tree

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------