Secure boot for imx6dlsabresd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secure boot for imx6dlsabresd

3,206 Views
DipinPK
Contributor II

Hi all,

I am working on a board with imx6dlsabresd processor and yocto 2.5 linux.

Now I am trying to implement secure boot feature for this and facing some challenges. Using the below link for implementing secure boot.

https://boundarydevices.com/high-assurance-boot-hab-dummies/

1. I am not able to activate Support i.MX HAB features feature for my u-boot and build it. It throws an error like invalid command (SECURE_BOOT). Our vendor informed me that we are missing HAB library to build this feature and need to get that from NXP. Is that correct?

2. Is the mentioned error is for missing HAB library? if yes how to get that and integrate with our BSP?

Thanks 

Dipin

0 Kudos
Reply
8 Replies

3,194 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

3,185 Views
DipinPK
Contributor II

Thanks for your reply.

I tried to enable the secure boot support using below method.

1.2 Enabling the secure boot support
-------------------------------------

The first step is to generate an U-Boot image supporting the HAB features
mentioned above, this can be achieved by adding CONFIG_IMX_HAB to the
build configuration:

- Defconfig:

  CONFIG_IMX_HAB=y

- Kconfig:

  ARM architecture -> Support i.MX HAB feature 

 But failed to build the u-boot after making configuration change.

Got an error like Invalid command (SECURE_BOOT).

Please help to build the u-boot with secure boot support enabled.

 

Regards

Dipin

0 Kudos
Reply

3,179 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dipin

 

this may depend on uboot version, as described on below patch

https://www.mail-archive.com/u-boot@lists.denx.de/msg373581.html

 

Best regards
igor

0 Kudos
Reply

3,177 Views
DipinPK
Contributor II

Hi,

My u-boot version is 2018.03

Regards

Dipin

0 Kudos
Reply

3,175 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

3,164 Views
DipinPK
Contributor II

Hi

Actually we have to use the existing version of u-boot as we have custom modification in that.

So it will be great if you can suggest some way to use the existing u-boot with secure boot feature.

 

Regards

Dipin

0 Kudos
Reply

3,158 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dipin

 

suggest to test procedure on some NXP i.MX reference board with uboot from

source.codeaurora.org/external/imx repository then repeat the same steps on custom

board.

 

Best regards
igor

0 Kudos
Reply

3,138 Views
DipinPK
Contributor II

Hi,

I am able to build the u-boot with secure boot feature enabled. But the below command not showing any HAB Block details..

The below is my command for that.

./tools/mkimage -n board/freescale/mx6sabresd/mx6dl_fs053_nt5cc256m16ep-ek-RA_Ver.cfg.cfgtmp -T imximage -e 0x17800000 -d u-boot-dtb.bin u-boot-dtb.imx

and this command shows output like below.

Image Type: Freescale IMX Boot Image
Image Ver: 2 (i.MX53/6/7 compatible)
Mode: DCD
Data Size: 663552 Bytes = 648.00 KiB = 0.63 MiB
Load Address: 177ff420
Entry Point: 17800000.

What is missing for my u-boot?

Why its not showing HAB Blocks?

Please provide your comments.

 

Thanks

Tags (1)
0 Kudos
Reply