Secure boot for imx6dlsabresd

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Secure boot for imx6dlsabresd

4,633 次查看
DipinPK
Contributor II

Hi all,

I am working on a board with imx6dlsabresd processor and yocto 2.5 linux.

Now I am trying to implement secure boot feature for this and facing some challenges. Using the below link for implementing secure boot.

https://boundarydevices.com/high-assurance-boot-hab-dummies/

1. I am not able to activate Support i.MX HAB features feature for my u-boot and build it. It throws an error like invalid command (SECURE_BOOT). Our vendor informed me that we are missing HAB library to build this feature and need to get that from NXP. Is that correct?

2. Is the mentioned error is for missing HAB library? if yes how to get that and integrate with our BSP?

Thanks 

Dipin

标记 (2)
0 项奖励
回复
8 回复数

4,621 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复

4,612 次查看
DipinPK
Contributor II

Thanks for your reply.

I tried to enable the secure boot support using below method.

1.2 Enabling the secure boot support
-------------------------------------

The first step is to generate an U-Boot image supporting the HAB features
mentioned above, this can be achieved by adding CONFIG_IMX_HAB to the
build configuration:

- Defconfig:

  CONFIG_IMX_HAB=y

- Kconfig:

  ARM architecture -> Support i.MX HAB feature 

 But failed to build the u-boot after making configuration change.

Got an error like Invalid command (SECURE_BOOT).

Please help to build the u-boot with secure boot support enabled.

 

Regards

Dipin

0 项奖励
回复

4,606 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dipin

 

this may depend on uboot version, as described on below patch

https://www.mail-archive.com/[email protected]/msg373581.html

 

Best regards
igor

0 项奖励
回复

4,604 次查看
DipinPK
Contributor II

Hi,

My u-boot version is 2018.03

Regards

Dipin

0 项奖励
回复

4,602 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复

4,591 次查看
DipinPK
Contributor II

Hi

Actually we have to use the existing version of u-boot as we have custom modification in that.

So it will be great if you can suggest some way to use the existing u-boot with secure boot feature.

 

Regards

Dipin

0 项奖励
回复

4,585 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dipin

 

suggest to test procedure on some NXP i.MX reference board with uboot from

source.codeaurora.org/external/imx repository then repeat the same steps on custom

board.

 

Best regards
igor

0 项奖励
回复

4,565 次查看
DipinPK
Contributor II

Hi,

I am able to build the u-boot with secure boot feature enabled. But the below command not showing any HAB Block details..

The below is my command for that.

./tools/mkimage -n board/freescale/mx6sabresd/mx6dl_fs053_nt5cc256m16ep-ek-RA_Ver.cfg.cfgtmp -T imximage -e 0x17800000 -d u-boot-dtb.bin u-boot-dtb.imx

and this command shows output like below.

Image Type: Freescale IMX Boot Image
Image Ver: 2 (i.MX53/6/7 compatible)
Mode: DCD
Data Size: 663552 Bytes = 648.00 KiB = 0.63 MiB
Load Address: 177ff420
Entry Point: 17800000.

What is missing for my u-boot?

Why its not showing HAB Blocks?

Please provide your comments.

 

Thanks

标记 (1)
0 项奖励
回复