Sabresd board : No HDMI output in Android JB 4.2.2 recovery mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Sabresd board : No HDMI output in Android JB 4.2.2 recovery mode

跳至解决方案
3,570 次查看
nickyeh
Contributor II


Hi,

I am trying to do android recovery mode in Sabresd board. In my environment, I use HDMI as output display, no LVDS.

Below is my U-boot bootargs:

console=ttymxc0,115200 init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 vmalloc=400M androidboot.console=ttymxc0 no_console_suspend androidboot.hardware=freescale

To enter recovery mode, I do folllowing steps:

1. copy sabresd_6dq-ota-.... .zip to /cache

2. create a file "command" in /cache/recovery, the contents of this file represent the filename of update package, it should look like below:

   "--update_package=/cache/sabresd_6dq-ota-....zip"

3. in CLI, execute "reboot recovery"

4. system reboot and get into recovery mode

In previous android release (imx-android-13.4.1), I can see rolling star in Android icon on HDMI display which represents the update process is running.

But In JB 4.2.2 ga release, No HDMI display, but I can confirms the recovery is running.

I had try to add "--show_text" in command file and it can display static pic, but cannot see like previous "rollong star" in Android icon.

Anyone can figure out what I miss?

Thanks in advanced.

标签 (2)
0 项奖励
回复
1 解答
2,318 次查看
nickyeh
Contributor II

Hi,

I got normal HDMI output in recovery mode while boot with below bootargs:

console=ttymxc0,115200 init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=16 vmalloc=400M androidboot.console=ttymxc0 no_console_suspend androidboot.hardware=freescale

The different is "bpp".

Anyway, I can modify u-boot to replace with this argument while system want to get in recovery mode.

Thanks

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,319 次查看
nickyeh
Contributor II

Hi,

I got normal HDMI output in recovery mode while boot with below bootargs:

console=ttymxc0,115200 init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=16 vmalloc=400M androidboot.console=ttymxc0 no_console_suspend androidboot.hardware=freescale

The different is "bpp".

Anyway, I can modify u-boot to replace with this argument while system want to get in recovery mode.

Thanks

0 项奖励
回复
2,318 次查看
nickyeh
Contributor II

Does anyone can help?

0 项奖励
回复
2,318 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Did you get an output in the HDMI in normal mode?

Have you tried with different panels? and changing the frequency?

Regards,

Alejandro

0 项奖励
回复
2,318 次查看
nickyeh
Contributor II

Yes, HDMI output work well in normal mode.

The problem in is JB 4.2.2 recovery mode, not in imx-android-13.4.1.

I am not sure the symptom could be duplicated in LCD panel since that is not required in my project.

I will do more experiment with different bootargs (resolution or something else).

Thanks your suggestion.

0 项奖励
回复