Use SPI on imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use SPI on imx6q

1,368 Views
levanthuan
Contributor I

I want to use spi for tranmit data path SPI1 SS0, Can I using function on uboot? Help me! Thank!

Labels (1)
0 Kudos
Reply
1 Reply

1,177 Views
AnsonHuang
NXP Employee
NXP Employee

Hi,

     I checked the i.MX6Q SabreSD board, there is a SPI NOR flash connected to CSPI1_SS0, so you can try using 'sf' command in uboot to write/read data on this SPI NOR flash, please see the help in uboot about 'sf' command and try it, thanks.

0 Kudos
Reply