SCM with onboard NOR Flash only

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SCM with onboard NOR Flash only

跳至解决方案
1,424 次查看
alexeytsirlin
Contributor I

Hi,

Is it possible to have Linux system operational with on-board 16MB NOR flash only? All the SCM user manuals describe booting from SD card process, but I cannot find any instructions about using on-board flash only. The SCM fact sheet states that "The 16MB SPI NOR flash is sized to support the storage of uboot, Linux kernel image, and an optimized Linux OS.", so I guess it is possible.

Thanks,

Alexey.

标签 (2)
0 项奖励
回复
1 解答
1,288 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alexey

please program images with Mfg Tools using script

mfgtool2-yocto-mx6scm-1gb-qwks-rev2-internal-spi-nor.vbs
Mfg Tool
Updates and Patches (2)
SCM-i.MX 6Dual/6Quad Manufacturing Toolkit for Linux 3.14.52 Patch Release (REV 1)
http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?f...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,289 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alexey

please program images with Mfg Tools using script

mfgtool2-yocto-mx6scm-1gb-qwks-rev2-internal-spi-nor.vbs
Mfg Tool
Updates and Patches (2)
SCM-i.MX 6Dual/6Quad Manufacturing Toolkit for Linux 3.14.52 Patch Release (REV 1)
http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?f...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复