SCM with onboard NOR Flash only

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SCM with onboard NOR Flash only

ソリューションへジャンプ
1,911件の閲覧回数
alexeytsirlin
Contributor I

Hi,

Is it possible to have Linux system operational with on-board 16MB NOR flash only? All the SCM user manuals describe booting from SD card process, but I cannot find any instructions about using on-board flash only. The SCM fact sheet states that "The 16MB SPI NOR flash is sized to support the storage of uboot, Linux kernel image, and an optimized Linux OS.", so I guess it is possible.

Thanks,

Alexey.

ラベル(2)
0 件の賞賛
返信
1 解決策
1,775件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Alexey

please program images with Mfg Tools using script

mfgtool2-yocto-mx6scm-1gb-qwks-rev2-internal-spi-nor.vbs
Mfg Tool
Updates and Patches (2)
SCM-i.MX 6Dual/6Quad Manufacturing Toolkit for Linux 3.14.52 Patch Release (REV 1)
http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?f...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,776件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Alexey

please program images with Mfg Tools using script

mfgtool2-yocto-mx6scm-1gb-qwks-rev2-internal-spi-nor.vbs
Mfg Tool
Updates and Patches (2)
SCM-i.MX 6Dual/6Quad Manufacturing Toolkit for Linux 3.14.52 Patch Release (REV 1)
http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?f...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信