SCFW 1.5.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SCFW 1.5.0

5,369件の閲覧回数
bmx666
Contributor II

NXP Android Q rev 2.2.0 is using SCFW 1.5.0. Is there any link for download or it not yet delivered?

ラベル(1)
タグ(1)
6 返答(返信)

4,380件の閲覧回数
uladzimir_liash
Contributor I

Hi, Bio_TICFSL Having same problem - need SCFW 1.5 sources

Plan to use Android 10 for our new development but definitely need to customize scfw core.

Have you any updates here? Any estimated dates or plans

Otherwise, we have to roll-back to Android 9 and decision should be taken quite fast

Thanks a lot!

4,380件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Sorry you have to way back to android 9. There is no source code available yet.

https://community.nxp.com/docs/DOC-342654 

Regards

4,380件の閲覧回数
vovchkir
Contributor I

Hello!

When will you  have planned release sources of scfw for Android 10?

Thanks!

4,380件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Maxim,

You can download the Q10.0.0_2.2.0-AUTO  and SCFW 1.5 from:

Android OS for i.MX Applications Processors | NXP 

Regards

0 件の賞賛
返信

4,380件の閲覧回数
bmx666
Contributor II

Hi Bio_TICFSL

Thanks for answer, maybe my question was not clear. There are only binaries like mx8**-scfw-tcm.bin, I asked about source code of SCFW 1.5.0 which delivered by SCFWKIT-1.5.0

4,380件の閲覧回数
vovchkir
Contributor I

And for our customer It will also be interesting 

0 件の賞賛
返信