SCFW 1.5.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCFW 1.5.0

4,018 Views
bmx666
Contributor II

NXP Android Q rev 2.2.0 is using SCFW 1.5.0. Is there any link for download or it not yet delivered?

Tags (1)
6 Replies

3,029 Views
uladzimir_liash
Contributor I

Hi, Bio_TICFSL Having same problem - need SCFW 1.5 sources

Plan to use Android 10 for our new development but definitely need to customize scfw core.

Have you any updates here? Any estimated dates or plans

Otherwise, we have to roll-back to Android 9 and decision should be taken quite fast

Thanks a lot!

3,029 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Sorry you have to way back to android 9. There is no source code available yet.

https://community.nxp.com/docs/DOC-342654 

Regards

3,029 Views
vovchkir
Contributor I

Hello!

When will you  have planned release sources of scfw for Android 10?

Thanks!

3,029 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Maxim,

You can download the Q10.0.0_2.2.0-AUTO  and SCFW 1.5 from:

Android OS for i.MX Applications Processors | NXP 

Regards

0 Kudos
Reply

3,029 Views
bmx666
Contributor II

Hi Bio_TICFSL

Thanks for answer, maybe my question was not clear. There are only binaries like mx8**-scfw-tcm.bin, I asked about source code of SCFW 1.5.0 which delivered by SCFWKIT-1.5.0

3,029 Views
vovchkir
Contributor I

And for our customer It will also be interesting 

0 Kudos
Reply