SABRE SDP MX6DL Android r13.4.1 Boot Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SABRE SDP MX6DL Android r13.4.1 Boot Issue

ソリューションへジャンプ
2,144件の閲覧回数
durmus
Contributor IV

Hi all,

 

I've recently received a SABRE SDP (IMX6DL). An SD Card with Android r13.4.1 image is also provided in the box.

I've inserted the SD card into SD3 socket and connected the power supply. A Freescale logo appears on the display but nothing more.

Then I connected USB debug cable, reset the board and observed the boot log via HyperTerminal (attached).

 

The last line is:

Freeing init memory: 220K

 

And it seems to get stuck there. I've searched it, come across with some issues. But none of them seems to be applicable.

 

Can someone identify the problem?

 

Thanks in advance.

Original Attachment has been moved to: SABRESDP-Boot-Log.txt.zip

ラベル(2)
0 件の賞賛
返信
1 解決策
1,616件の閲覧回数
durmus
Contributor IV

If anyone is interested in this, I have come to the conclusion that the SD card was corrupted. I reformatted it using i.MX6DL_SDB_SD_Demo_Image.exe on Windows (just select Physical Drive rather than Removable).

Then the demo image booted just fine. Here are some topics that might be helpful:

Problem with i.MX6Q_SDB_SD_Demo_Image.exe

Mfgtools does not create Android SD card similar to one provided in kit

MX6Q-SDB - installing Linux (Win user)

i.MX6DL SABRE platform prebuilt Android jb4.2.2 image issue

Cheers.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,617件の閲覧回数
durmus
Contributor IV

If anyone is interested in this, I have come to the conclusion that the SD card was corrupted. I reformatted it using i.MX6DL_SDB_SD_Demo_Image.exe on Windows (just select Physical Drive rather than Removable).

Then the demo image booted just fine. Here are some topics that might be helpful:

Problem with i.MX6Q_SDB_SD_Demo_Image.exe

Mfgtools does not create Android SD card similar to one provided in kit

MX6Q-SDB - installing Linux (Win user)

i.MX6DL SABRE platform prebuilt Android jb4.2.2 image issue

Cheers.

0 件の賞賛
返信