SABRE On screen keyboard Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SABRE On screen keyboard Issue

ソリューションへジャンプ
1,767件の閲覧回数
lijothomas
Contributor II

Hi all,

Completely new to the iMX world, procured a SABRE board for our development activity.

Ported linux successfully using LTIB and Yocto environments .

The on screen board functionality is not working,  tried to add lot of stuffs but nothing works.

Could anyone suggest any methods to get the on screen keyboard for the SABRE platform.

Thanks in Advance !!!!!!

Regards

Lijo Thomas

ラベル(1)
0 件の賞賛
返信
1 解決策
1,649件の閲覧回数
art
NXP Employee
NXP Employee

Try the latest L3.14.28 Yocto Linux BSP by Freescale, available for free download on the i.MX6 SABRE SD Software&Tools web page (check the "Board Support Packages" section):

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT&fpsp=1&tab=Design_Too...

Everything works well there.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,650件の閲覧回数
art
NXP Employee
NXP Employee

Try the latest L3.14.28 Yocto Linux BSP by Freescale, available for free download on the i.MX6 SABRE SD Software&Tools web page (check the "Board Support Packages" section):

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT&fpsp=1&tab=Design_Too...

Everything works well there.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------